Hi, I'm looking for a replacement of Non-Isolated POL DC-DC converter.
Part no: PTN04050AAH
Please suggest Drop-in.
My requirements:
Input:2.3V to 7V
Output: -3V to -12V adjustable. (-3V, -5V, -12V)
Output Power:6W
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mahesh,
Thanks for using the e2e forum.
PTN04050AAH is obsolete and no longer available.
From the same family, PTN04050C is still available:
https://www.ti.com/product/de-de/PTN04050C
Please check if this device fits your application.
Aside from this part, there are no other modules available this our product family.
Instead, an inverting buck-boost could be used, e.g. TPS62913.
Best regards,
Niklas