Other Parts Discussed in Thread: TPS92511,
Hello guys,
One of my customers is looking for LED driver which can be used for the following conditions.
Topology: 1channel Buck
VIN: 18V~40V
LED total Vf: 9~11V
Iout: 100~200mA
Dimming method: PWM
We recommended to use TPS92511 to the customer.
But they wanted to use a new LED driver which was released within 10 years because their product life time is more than 10 years from the product releasing.
So I am thinking of recommending TPS922052 to them.
I have the following questions about this device at this moment.
Could you please give me your reply?
Q1.
Their driving current is 100~200mA.
Is it no problem for TPS922052 to driver 100~200mA though the current is smaller than the device current capability?
Q2.
If you have any other LED driver which suits to their requirements, could you please tell me?
Your reply would be much appreciated.
Best regards,
Kazuya.