Other Parts Discussed in Thread: TPS61027, , TPS61023, TPS61032, TPS61030
Hello,
I want to use TLV61070 as voltage converter, input voltage from 1.8V to 3.2 V, want to output 5V/1A.
the schematic as picture, I use 2.2uH(74438357022) inductor, but circuit work abnormal, can not output 5 V voltage, the output voltage alomost as same as input voltage .
could you help check where the issue of this circuit?(please ignore D41, R20, C12, they are unwelded)
Note, I use a bread board to weld the circuit.
Thanks.