This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21222: Suggest the isolated gate driver part for our design

Part Number: UCC21222
Other Parts Discussed in Thread: UCC21231, UCC21225A

The following are our design requirements for the gate driver. Please suggest the gate driver part which is suitable for our below design requirements.

Isolation Type : Basic Isolation

Input Bias Supply Voltage : 3V to 5.5V

Output Bias Supply Voltage :  12V Range

Number Of Outputs : 2(Half bridge configuration)

Output peak source current : 5A to 8 A

Switching Frequency : 250 KHz

Degree of Contamination : Class II as per IEC 60664-1

Over Voltage Category : Class II as per IEC 60664-1

Isolation Resistance(input to output) : >1Meg Ohm

Mounting style : Surface Mount