Hi team,
I wanted to know if reading the register 0x02, will give the exact battery battery temperature and is it possible to identify under temperature, over temperature conditions during charging.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I wanted to know if reading the register 0x02, will give the exact battery battery temperature and is it possible to identify under temperature, over temperature conditions during charging.
Thanks
Hello Aldrina,
Reading from the 0x02 register will return either the temperature measured from the gauge's internal thermistor, or the temperature from an external thermistor. Whether the gauge reports the temperature from the internal or external thermistor depends on the OpConfig [TEMPS] bits. Please see the following image taken from the bq27426 TRM.

Regards,
Jonny.