This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM5601R5H: Support for transient Iout higher than 1.5A

Part Number: TPSM5601R5H

Hey Power Module team,

I have a customer evaluating the TPSM5601R5H power module for a project and we are hoping you could help to provide feedback on the following inquiry:

The datasheet for this module shows 1.5A Iout Max in the Recommended Operating Conditions table. We need a supply supporting a mean current of 0.4A that can also support a peak current of 1.75A for 100ms. How would this module behave in that scenario? We like it for its compactness. Do you have any other power modules similar to this supporting 16V-60V input and 12V output with 2A peak current capacity?

If there are any on the roadmap that would be a perfect fit that you cannot comment on in this thread feel free to reply back to me directly over email.

Thanks!

Best regards,

Matt Calvo