This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55010: Low Iq isolated DC-DC

Part Number: TPS55010


Hello, I'm looking to develop an isolated DC-DC with input of 3.3V and output of 12V with a maximum output current of 50 mA. The main consideration of this is low standby current drawn from input without any load on output - less than 500 uA.

Would this be possible with TPS55010 or do I need to use any other chipset?

Regards, Prithvi

  • Hi Prithvi,

    Thanks for using E2E.

    The TPS55010 is the correct device for your requirements. You can use the WEBENCH tool on ti.com for the schematic and simulation:

    https://webench.ti.com/power-designer/switching-regulator/customize/30?VinMin=3.3&VinMax=3.4&O1V=12&O1I=0.05&base_pn=TPS55010&AppType=None&Flavor=None&op_TA=30&origin=pf_panel&lang_chosen=en-US&optfactor=3&Topology=Flybuck&flavor=None&VoltageOption=None

    Best regards, 

    Sepp