Other Parts Discussed in Thread: LMR33620, LMR43620,
Hi support team,
This is a question about TPS62933FDRLR.
If 2pin (EN) and 3pin (VIN) are short-circuited, it is assumed that a voltage exceeding the maximum rated voltage of 2pin (EN), 6[V], will be applied.
Is there any possibility of fire or smoke occurring at this time?
VIN voltage is 24V.
Are there any devices that take measures against short-circuiting of pins adjacent to VIN, where the maximum rating of the pin adjacent to VIN is set higher than VIN?
Regards,
Dice-K