Dear All,
I am trying to make an interleaved PFC using UCC28070. Presently I am at the schematic design stage. I need for operation in 3kW power level at 230 V input. I doubt the current sense network. I am highlight the part in red. Why is it linked to the gate circuit? Also whether the highlighted part with blue is sufficient for the implementation of the circuit.
Please note that i will be using PE-63588NL current sense transformer and UCC27517ADBVR for gate driver. The schematic where I am having doubts is attached. Also whether this current sense transformer which I mentioned is applicable for this power range.