This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Disable Source role to save power question

Part Number: TPS25750
Other Parts Discussed in Thread: TPS25751

Hello Everyone,

I am using the TPS25750 as dual (sink and source) roles, and I want to disable the source capability to save power (like a power saving mode).

I do not understand from the User Guide (https://www.ti.com/lit/ug/slvuc05a/slvuc05a.pdf?ts=1709200793179&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTPS25750) how to do it...

I thought that reducing the number of Source PDOs to 0 in register 0x32 (first 3 bits of the first byte) and sending the "SSrC" command should work, but it didn't. Then I tried also to put also the maximum current to 0 (first 10 bits of the PDO's bytes), my phone (attached to the TPS via USB-C) starts activating/deactivating the battery charge constantly.

What am I doing wrong? 

Thank you in advance