This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: Looking for Power Path Controller Recommendations

Part Number: BQ25750
Other Parts Discussed in Thread: BQSTUDIO

Hello,

I am currently working on an application that utilizes a 4-Series LiFePO4 battery pack that runs a system when there is no power input.

I have looked through the catalog of lithium charge/power path ICs and I am struggling to find the correct one for my application.

The chipset will need to stand-alone and not need an external controller to work.

The minimum charge for the pack would be 2A, and the main power rail would need to handle 16A.

What chipset would you recommend to use?