This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Device Comparision Table and Data Memory Setting

Part Number: BQ76952

Hi


I'm planning to use BQ7695202, but for now I'm checking using BQ76952(EVM).

For the firmwear of host, is the difference between two devices only in what is written on Device Comparison Table?

"REG1 LDO Default" is set to "Enabled, set to 3.3V".
Does this mean that the Data Memory Settings are as below?

・Settings:Configuration:REG12 Config
 REG1V_2–REG1V_0 = 6(3.3V)
 REG1_EN = 1(REG1 Enabled)


・Settings:Configuration:REG0 Config
 REG0_EN = 1(Preregulator is disabled)