This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54A24: Unable to configure the transient pulse current setting in Webench

Part Number: TPS54A24


I'm currently encountered with issue which couldn't configure transient pulse current setting in Webench. Setting would like to configure as below:

Initial Load Current: 6.3A
Minimum Load Current: 0.7A
Initial Time Delay (s): 0
Fall Time (s): 0.0000224
Rise Time (s): 0.0000224
Pulse Width (s): 0.01