Other Parts Discussed in Thread: LM74930,
Hi!
I want to use LM74930 as ideal diode from PS normally up to 60V.
There may be peaks up to 100V
1. Is LM74930 suitable for this application?
2. If I use LM74930 with load dump feature, will it protect output for at least 80V max if done properly?
I mean can I put 80V logic after this switch or I should anyway stay with 100V rated electronics?
Stas