This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: BQ25713: ADC conversion on battery supply not triggering

Part Number: BQ25713

Hi,

Using the BQ25713, i want to do ADC conversions when only supplied by battery.

It is stated in datasheet that "When enabling ADC, the device exit low power mode at battery only":

It doesn't seem to work. When I trigger ADC only supplied with battery with commands:

{0x3B, 0x60}

{0x3A, 0x01}

The conversion is not done. I think device doesn't exit low power mode ?

To trigger ADC I should manually exit low power mode:

 {0x00, 0x60}
 {0x01, 0x0E}

Then only I can do  ADC conversion on battery mode.

Is it normal ? To be sure to read the last ADC result should I make device exit low power mode every time before a conversion ?

---

The workaround I thought was to send a reset command: RESET_REG

{0x35, 0x40};
{0x34, 0x30};

so the ADCVSYSVBAT goes to 0, so I know if a conversion has been done or not. But the ADCVSYSVBAT doesn't seem to be resetted. It keeps the last conversion.

Again, is it normal ? Do you think to any other workaround ?

Thanks in advance.