This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256304: configurable output

Part Number: UCC256304
Other Parts Discussed in Thread: PMP, UCC256403,

I am looking at the PMP21863 application note which is configured for a 48V output.

I want to change the output to 57VDC. can I just change the resistor divider at the reference point? teh application note design is for 48V and 11A for a total power of 528W. I am looking at a 500W output at 57V.

Do you think this can be done? also can i get one of teh boards used in this design?

Thanks.