Other Parts Discussed in Thread: TINA-TI
Howdy. I've been trying to do a transient simulation in TINA-TI on a boost converter using the LM5122. I can get the simulation to run for about 28 microseconds and then it dies with a convergence error. Said errors ALWAYS involve one of the semiconductors (e.g. component T2.DBD).
I have attached the TINA-TI schematic file. The design is a verbatim copy of what Webench suggested for my design given the input and output voltage & current parameters I entered.
I'm guessing maybe the spice files for the semiconductors might be goofy, but they came straight from the manufacturers (in the case of the MOSFETs they are from TI). I've tried adding body diodes in parallel to the MOSFETs, that made no difference. I've also tried fiddling around with the piecewise linear voltage to ramp it at different rates, that made no difference either. So, I'm kind of out of ideas on what to do.
Any help would be greatly appreciated. Thanks.lm5122_boost_conv2.TSC

are straight out of Webench (see attached screenshot). That the circuit will not function with the design that Webench supposedly created and validated is rather frustrating. Maybe that's why it failed to export the Tina model? LOL.