Hi
I am worked with BQ24610. I am given the input voltage 18 v and getting system voltage 18V. As par evaluation board i am getting all the voltages correct on IAset,Iset1,Iset2 pins. But when i am connect the battery i got 10V Vbat for some time.(R25=470k) But after 2-3 min Vbat goes to 0.9 volt.I connect the JP1 (jumper) to pin 1-2 and also check for 2-3 But same results occurs.My STAT1 and STAT2 led's are also don't glow.If I connect fully charged 12 v Battery then D3 is glowing but stat1 and stat2 are not glowing. If anyone knows about this problem please told me.
Thanks and regard
nilesh