I have some issue which no start up at full load(5Vin 3.3Vo 20A), the circuit has two same FET in upper and bottom side.
The start up is ok at 50% load condition, but fails at full load, so I am wondering it happens shoot through due to same Qg FETs(Qgd/Qgs >1).
The problem is gone if boot resistor increase, but efficiency hurt a little bit, so I am considering to change bottom FET with a FET of big Qg than upper FET and Qgd/Qgs<1.
The controller is TPS40041. I'd appreciate if somebody give some advice, Thanks.