This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8863-Q1: Default Brightness Values at Maximum

Part Number: LP8863-Q1


Hi, 

The LP8863-Q1's current and brightness values for the LED channel registers are maximum (0xFFFF) by default.

I am currently using the EVM board and an Arduino via I2C but wish to include this driver in a PCB design.

When I power the driver, the LEDs all light up to maximum for a second before the arduino code kicks in to change the brightness values. I wondered if this could be prevented in some way? Perhaps by changing the default max values, or managing the start up sequence? 

Many thanks, 

Genevieve