Hi Team,
I am facing some issues while programming TPS544C26 IC using I2C GUI in Fusion Software.
My desired Vout is 1.8V, Protocol ID is 10mV VR13.
1. a. When I am setting VOUT_CTRL as I2C only, Protocol ID as VR13, 10mV and VOUT_CMD as 0.9V, I am getting output voltage on board as 1.8V(checked with multimeter), whereas graphs in GUI shows 0.9V.
Whatever value is set in VOUT_CMD command, getting double at output voltage after checking with Multimeter.
This looks like when I am setting 83h in VOUT_CMD in A6h, I am getting 1.8V on board which is for 10mV but GUI is showing 0.9V which is for 5mV.
b. When I am setting VOUT_CTRL as SVID only, Protocol ID as VR13, 10mV and VBOOT as 1.8V, I am getting output voltage on board as 1.8V(checked with multimeter) and graphs in GUI is also showing 1.8V as attached below. So this case is working fine for us.
2. When I am trying to set PROTOCOL ID as 5mV, I am getting NACK.
Why I am not able to set 5mV in Protocol ID register?
Thanks,
Siddhi