Hi,
I have some questions as below, please help to confirm, thanks!
Q1: the UCD9090 could support I2C/ SMBus and PMBus three types interface, right?
Q2: Regarding to the Fault log stored in flash, is there limitation for flash stored times?
Q2-1: If the error log continues to appear and is cleared, will it cause UCD9090 crash?
Q2-2: When the times over 10000 or more, what happen on UCD9090?