This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2490: MOSFET Junction Temperature query

Part Number: TPS2490

Hello,

For TPS2490, I have selected a MOSFTE SQJ138EP.

While calculating the junction temperature from case temperature, on page 9 below equation 9 is given in datasheet -

With this equation the case temperature is 209 degrees C which is well above the absolute maximum Tj rating of MOSFET (Tj max = 175 deg C)

So Can I assume Tase > 30 deg above ambient (say ambient = 90 deg C)

With this, my junction temperature is well within the limits.

Regards,

Abhishek D.