I am looking for a synchronous buck converter, 6-9V input to 3V (adjustable) output, 3-4 A. As EMC compliance is an issue in my application, I'd like to use a converter with low radiated noise. I was looking for a TPS54527, which has the FETs integrated - this means there is no way of influencing switching speed (like reducing speed in order to reduce noise). Is there any EMI data available from TI? Or recommendations which families are better suited for reduced EMI? The only way I see right now is to purchase an eval board and do measurements with the spectrum analyzer.