Other Parts Discussed in Thread: TPS55288
Refer to attach file as PD control block diagram.
1.How the process control from TPS65987D and Qualcomm and USB-C plug insert?
2.Especial with USB0 for Qualcomm chip need detect VBUS insert event.
My scenario is
(1)USB0(USB3.1) normally for PD output 5V~20V,
(2)TPS65987D after finish communciate by CC pins with TypeC connecter insert, does it can notify to CPU(QCS6490) and controlTPS55288 for DC/DC output 5~20V adjustable?
(3)TPS25730D behavior similar as item(2)
(4)If defailt without any image(code) inside the meory, Qualcomm PMIC(PM7250B-2) need detect VBUS insert and triggle SW code. Refer below block diagram blue circle area, does TPS65987D need insert VBUS power for workable and can detect CC pins. Or refer to block diagram, anything design incorret on TI section.
Please let me know your commect, thanks in advance.