Hello TI Team,
We are implementing a DC-DC converter where our input voltage is 34 Volts and we are trying to get dual output of +22V and -6V. We are using the excel sheet given by the TI for LM25184.
Our transformer is a customer designed transformer with 1:5:1:0.278 +-3%. Currently the output voltage we are getting is +32V and -8.45V. It looks like there is a feedback problem, but I have checked with different resistances but still getting the same voltages. The design sheet is also attached here for the selected requirements. Can you please have a look and let me know what can be done to get the right voltages. Thanks