If REGIN and BREG pins are connected to the ground, then is it possible that there will be a short circuit upon powering BAT+ and BAT- (naming based on reference design)? Because in my circuit when I supply 30V from the power supply at a max limit of 0.7A the circuit goes into CC