Other Parts Discussed in Thread: BQ25750, BQSTUDIO, EV2400
Hi TI team,
I use BQ25750 EVM in a standalone operation without BQStudio.
I change R67 from 4.99K to 12k.(ICHG 10A-->4.16A)
Load: EL CV mode
Q1: VBATLOWV not in the SPEC.
Calculated the value of VBATLOWV is 18.54V~20.72V.
EL CV mode: Precharge -> fast charge @ Actual value: 21V (not in the 18.54V~20.72V)
Load: 7S1P 18650 Battery
Q2: When the CV mode, ICHG spikes.
Precharge -> fast charge -> Termination
Q3: Termination current not in the SPEC.
Calculated the value of termination current HW Limit (ICHG pin) : 10% x ICHG = 10% x 4.16A = 0.416A
Actual value: 0.284A
Thank you,
Regards