Hi team,
Customer wants to reduce footprint including passive components. So asking some questions.
What is the main purpose of Cout? reference is 470uF, can customer decrese it when Iout is 1A?
If they don't need some function of LM7310, is the floowing pin condition is correct?
Not use UVLO: resistor btw IN and EN/UVLO is not needed.
Not use OVLO: Resistor btw OVLO and GND is not needed.
Not use PG: leave floating
Not use PGTH: Leave floating
Not use DVDT: leave floating
Not use IMON: Connect IMON pin to GND
Regards,
Hayashi