This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: TPS53355

Part Number: TPS53355
Other Parts Discussed in Thread: TPS546E25

Hello,

We are now trying to replace out power solution from LTM4671 to TPS53355.  One problem is as belows:

We hope the voltage decreasing is below 15mv when the load(50%) is coming. 

As a result, we can apply a Type II C-R-C compensation network to improve the Transient Response, especially the decreasing in voltage when the load is coming.

However, we can not find any similar options in TPS53355.

Dose TPS53355 support ? 

If not, can you recommand other Ti device?