Hi,
i intend to use LM61495 for (15-32v 24 nominal) 24v-12v conversion at 0.6A\0.3A (max load\light load).
would you recommend this use? , could you estimate the efficiency of this solution? (using 400Khz switching frequency)
also, assuming that the solution will conduct in light mode - does this change the inductor selection proses? (or still the eq in the datasheet regarding ripple and min value are still valid)
note that, when simulating in PSPICE I've got a waveform matching CCM conduction mode, while I was expecting DCM / frequency reduction ( ive used the PFM version).
best regards,
Tomer Ashkenazi