Other Parts Discussed in Thread: TPS65130, UCC12050, TPS65132
Hi,
In my new design, we select UCC33420 which can support 300mA (totally 1.5Watts) isolation power, but in my test, the output is prohibited when the output current is over 100mA, please see below plot. in our application the following is DC-DC chip from TI, the total current is ~120mA@5V VCC isolation voltage. please help check it, thanks.

best regards,
Jay




the zoom in is attached, and captured yesterday. due to the ossciloscope limitation, the picture is not very clear. thanks.