Other Parts Discussed in Thread: LM5156
Hi expert!
I want to know if I add 330nF CUVLO in parallel with RUVLOB. Should I add RUVLOS? I don't know if this capacitor is too large...Or what is your recommendation for this capacitor? Vsupply is 12V battery.

- RUVLOT=14.7K, RUVLOB=6.81K, Vsupply= 6~16V
- RUVLOT=14.7K, RUVLOB=11.3K, Vsupply= 6~16V
Can you help with this two combo if there are difference of RUVLOS?
besides, where can I find/calculate total power loss of LM5156H-Q1 as a flyback controller?
Many thanks!