Other Parts Discussed in Thread: LM5181, LM5180
Hi
I am Frank ,recently we have to use the LM5017 flyback constructure application (40-55V/input) to (13V/Output) and ISO 5V/5V/12V , and I measure the power comsumption is 6.1mA without iso part only 13V non-iso when there is no load
is there posible that can reduce the power comsumption in no load thougth modify the parameter component ex: Ron-Vin Resistance etc.... or change the frequency?
1. is there any wayreduce by modify?
2. if not is that any solution which TI recommand ? another flyback IC??