This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD19536KTT: this mosfet and other mosfets also are not having thermal resistance for minimum copper and 1 sq inch

Part Number: CSD19536KTT


CSD19536KTT for this mosfet can someone provide thermal resistance for minimum copper layout  and 1 sq inch pad layout  so that we can calculate power dissipation for them.

  • Hello karan,

    Thanks for your interest in TI FETs. TI only specs RθJA and RθJC in the FET datasheet. As shown in the blog at the link below, RθJA is measured with the FET with the device suspended in free air (no forced convection). RθJC is measured to the drain tab. I have checked some other vendors datasheets for D2PAK FETs and they spec RθJA = 40°C/W with the device surface mounted on a 1in² Cu pad. It should be about the same with the TI FET. Please let me know if you have any questions.

    https://www.ti.com/lit/ta/ssztb80/ssztb80.pdf

    Best Regards,

    John Wallace

    TI FET Applications