This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS610981: Best device for application

Part Number: TPS610981
Other Parts Discussed in Thread: TPS61299A, TPS61299, TPS61322, TPS61099

Hi,

I'm currently using the TPS610981 which has a 3.3V output but I need to change to something with a 5V output but there are so many devices to choose from.

I have a circuit running from 2x AA batteries in series = 3V and I want 5V out to power 5 WS2813B LEDs and an ESP12, I want to use a LDO from the 5V supply controlled from the ESP12 to power the LED supply.

The device will spend the majority of it's time in deep sleep @20uA and peaking to around 400mA when activated.

Can you advise the best step up converter to use?

Thanks