Part Number: UCC24612
Hi team,
I have question related to Adaptive Blanking Time of UCC24612.
Following the datasheet, there is Adaptive Blank Time function which prevents false turn-on of the device occured by DCM ringing. It seems the blank time is decided to have the value which is calculated by (N-1) SR_OFF time * 70% but in Samsung board, there is false turn-on before the blank time ends. Details are as below:

TOFF(N-1) = 4.772us so, blank time would be calculated as 70%*TOFF(N-1)=3.34us but as you can see from the below waveform, the SR turned ON with blank time 2.21us which is much less than calculated value 3.34us. Also, it doesn’t make sense comparing with the spec of tOFF_MAX, 2.65us.
I think I might have misconfigured the oscilloscope point 1,2 to measure the blank time or real waveform doesn't follow the datasheet. Could you tell me the exact criteria for measuring blank time in the waveform below? or any idea why measured value is different from the datasheet?