Other Parts Discussed in Thread: TPS63806,
Hi, i'm designing a power board which has a 3.3v line from a lithium ion cell. The system should consume less than 1mA on sleep, and 3A on peaks, which this chip doesn't support (at least datasheet doesnt say). The board has a very constrained space, so i cant add a bigger inductor, but i can add multiple small ones.
I want to explore the possibility of putting two of these in parallel.
Is it possible?
Thanks,
Andres