Hi, can you please assist with this customer question regarding TPS23881:
We are using the part in a 4-Port 4-Pair configuration. Our design slightly differs from the recommended application (figure 10-2) in the datasheet with respect to the fuses. Instead of having individual slow blow fuses in the return path of each coil, we have a single one at the supply (+54V) for both coils, i.e. one fuse for each RJ45. The fuse we are using is the TPS26600RHFR eFuse.
The Issue... For some reason, whenever a fuse is triggered the TPS23881 is reset. I have observed both the RESET pins and +3V3 rail during this, and can confirm no glitches appear. Upon reset the TPS23881 also reverts from its loaded firmware (v14) for the original (v0) but I think that's to be expected.
Our circuit:
Many thanks,
Tristan