Other Parts Discussed in Thread: LM5171, LM5170
Hi,
I want charge 100V lion battery with boost topology and CC-CV. Is LM5121 suitable for battery charging? If not, do you suggest any design?
Vin: 40V-56V
Charge current: 2A
Battery pack voltage: 100V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Musa,
Thanks for reaching out to us via e2e.
The LM5121 is a booster which can only regulate on a constant voltage output.
Constant current operation is not possible with the built-in features.
Maybe have a look at the LM5171 or the LM5170.
Best regards
Harry.