This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: BQ27441-G1: How to configure for a new battery (UFX 605080)

Part Number: BQ27441-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400, GPCCHEM

I am trying to configure the fuel guage with the Li-ion Polymer.

1. Where can i find the list of closely matched chemical ids ?

Nominal Capacity = 3000 mAh

Typical Capacity = 3050 mAh

Min Capacity = 3000 mAh

Cell initial Impedance <50mohms

Nominal voltage = 3.7 V

Initial Voltage  => 3.8V

Limited Charge Voltage = 4.2 V / Cutt off voltage = 3.0 V

Temperature range = 10 -55 C (Charging) ,~20 -60 C (Discharging)

want to operate from 3.3 V to 4.2 V range.