This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568A: PG pin sink current limit

Part Number: TLV62568A

We are using TLV62568AP buck in one of our designs and the PG pin is used as enable to a load switch as shown below. 

Can I connect the PG to EN directly or should I add R11 as shown? In the datasheet, it is given sink current of PG pin is 1mA max. While adding R11, I am getting other issues with the load switch.