This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010935: design consideration

Part Number: TIDA-010935

Hi expert,

May I learn from you what if customer want to have PLC through 5V cable instead of 12V referring to the TIDA-010935 design, what circuit do we need to modify and/or anything need to be considered?

Thanks,

Allan   

  • Hi Allan,

    the voltage on the power line itself does not have a big impact on the PLC circuit itself, just the coupling circuit. TIDA-010935 will also work on a 5V power line.
    In our design we have we generate the 12V supply from the power line itself, which is greater than 12 V with a buck converter. If you want to generate the 12V supply for the power amp from the 5V power line, you need a boost converter,

    Best regards,

    Andreas