Other Parts Discussed in Thread: PSPICE-FOR-TI, TLVM13630
Tool/software:
Hello: I am trying to perform transient simulation of a switching power supply using the LM20333. The available model is for TINA SPICE, so that is what I am using.
However, the basic simulation will not converge. I have using values off the data sheet for a 12V input being switched down to a 3.3V output. The sim starts showing no errors such as disconnected nodes or wires. I have tried many variations of adjusting the transient parameters PIVREL, PIVTOL, and maximum iterations. I've also tried applying initial conditions and switching between trapezoidal and gear integration. Nothing affects the transient simulation in the slightest. It runs out to 38% completion on a 1ms run, and then hangs with failure to converge.
Can you provide any advice on getting this model to run? The file I am using is added below.
Thanks,
Farron