Tool/software:
The following description is found in the “Table 8-1. Buck output capacitance” section of the datasheet
MAX (Includes local + point of load)
I have two questions about this statement
(1) What does “point of load” mean?
Does it refer to the noise limiter capacitor used in the LSI that uses the power supply generated by the TPS6521905?
(2) What kind of problem will occur if I install a capacitor that exceeds the Max Capacitanse shown in Table 8-1?
Best regards.