This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596S-ADJEVM: EMC Compliance standard

Part Number: LM2596S-ADJEVM
Other Parts Discussed in Thread: LM2596, , LMR33610

Tool/software:

 EMC Specification
S.NO EMC Standards Required Class/Levels
1 Emission Conducted Emission Class A
2 Radiated Emission Class A
3 Immunity ESD 1. 6KV Contact
2.  8KV Air Discharge
4 EFT  2KV
5 Surge 1KV, 25A
6 Radiated Succeptibility Level 3 = 10V/m 
7 Conducted Succeptibility Level 3 = 10V(r.m.s)

The above is the EMC standard levels which i'm folowwing inorder to get my prodoct CE certified.

Additional Info on product :

1. This is an ITE(Information Technology Equipment)

2. Operating Voltage : 24Vdc

 I need to ensure that the above standards are met by LM2596 inorder to impliment in design.

Couldn't get hold of the information from datasheets.

Also where i can get CE certificate & test report of this DCDC convertor(LM2596S-ADJEVM), if it is CE certified.

Any suggestion regarding this is welcomed.