This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26630-33EVM: TPS26630-33EVM

Part Number: TPS26630-33EVM

Tool/software:

Hi,

On the eval board there is a voltage divider for the PGTH function (PGOOD comparator).

The eval board is supposed to work over the range 4.5-60V.

That makes the voltage at PGTH 0.45V to 6V. 

The datasheet says the PGTH threshold is about 1.2V.

How is this supposed to work over the entire range??

Dan