Part Number: MC34063A
Tool/software:
Hello,
When I try to calculate inductor value, I can not find Vsat. External capacitor is not used.
Please can you explain about Vsat.
What is the frequency value of step up referance design on datasheet ?
may I calculate switching frequency using Ct and Rsc? does it vary depending on input voltage?
And another tricks point which a needed?
I am trying design two circuit.
1_>> Vin: 8-35 VDC, Vout:37 VDC, L<=100uH >> f=?, Co=?, Rsc=?, Ct=?, L=? (frequency should be as small as possible)
2_>> Vin: 8-35 VDC, Vout:6 VDC, L<=100uH >> f=?, Co=?, Rsc=?, Ct=?, L=? (frequency should be as small as possible)
İf Vin varies between 8 and 35 volt, how can I choose the correct values.?
Best regards.