Other Parts Discussed in Thread: LP5812
Tool/software:
Hi Team,
We are planning to use LP3943 LED driver in our custom board and the application is to blink the all of the LEDs from the u-boot of SK-AM64 base custom board.
I've identified some of the resistors to blink based on the datasheet(1Hz and 50% duty cycle).
PSC0 = 0x09F
PWM0 = 0x80
LS0, LS1, LS2, LS3 = 0xAA
Among the queries I have are
- After it is set, does it blink during the boot process (until kernel prompt)?
- When we blink, do we experience any delay or flickering effects between the LEDs?
Thanks,
Dharmik