This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: The value of resistor connected to the BATP

Part Number: BQ25798

Tool/software:

Hi Team,

It is written in the datasheet that, "Place100Ω series resistance between this pin and the battery positive terminal".

I saw on another E2E that this resistor can protect the battery from short circuit issue. It seems that a larger resistor can limit the current more effectively.

Will replacing this resistor with a larger value (like 240ohm) have any other effects?

BR

Adrian

  • HI Adrian,

    Possibly. No higher than 100 Ω is recommended because the BATP pin pulls uA of current into the SDRV charge pump when only battery is connected.  We do not want more and have not tested for a higher voltage drop on that resistor.  

    Regards,

    Jeff